eo_logo
  • Country/Region
  • cart   
 

Glossary: V

Varifocal

Low magnification lens which has a variable focal length, but which requires refocus with adjustment.

Vernier

For rotary stages, a scale measuring the amount of angular movement by the drive. Vernier values of resolution are the smallest angular movement that can be measured by the scale.

Vibration Rating

Measure of the vibrational durability of a component within a certain range of frequencies, expressed in units of acceleration (G).

Viewing Angle

For light control film, the full angle through which the film will transmit light. This value is centered about the louver angle of the film.

  See also Louver Angle

Vignetting

A fall-off in illumination of the image.  This can occur when the sensor is larger than the specified maximum sensor size of the lens is used or can naturally occur due to limitations of the geometry of the system.

VIS Coating

BBAR coating optimized for use in the visible spectrum between 425 nm and 675nm. Does not transmit NIR efficiently.

VIS/NIR Coating

BBAR coating optimized for use from 425nm to 900nm with good transmission out to 1000nm.

Viscosity

A measure of a fluid's resistance to flow, or the ratio of shearing stress to the velocity gradient.  Water is a low viscosity fluid while peanut butter has a high viscosity.  

Visible Spectrum

The part of the electromagnetic spectrum from approximately 400 - 750nm. 

Spherical optics, aspheric lenses, prisms, imaging lenses, imaging and laser optics assemblies, and mechanics are just a few of our expertise.

Edmund Optics' engineers are experts in delivering the best solution possible. From stock products to custom designs, EO has the industry and technical knowledge to help meet your needs.

Over 15 regional offices in the Americas, Europe, and Asia to offer local support with world-class service.

Need to contact Edmund Optics? Use any of our fast and friendly services to meet your needs.

Sales & Expert Advice
 
or view regional numbers
Easy-to-Use
QUOTE TOOL
enter stock numbers to begin


×