Edmund Optics® (EO), the premier provider of optical components, announces the TECHSPEC® Nd:YAG Harmonic Separators. These beamsplitters are used to separate the common harmonic wavelengths of an Nd:YAG laser. The precision mirrors are designed for a wide range of demanding Nd:YAG laser applications.
TECHSPEC® Nd:YAG Harmonic Separators are dichroic mirrors used for separating the harmonic, frequency-doubled beam from the pump beam, which is often outside the laser resonator. The frequency doubled light is reflected to nearly 100%, while most of the pump light is transmitted.
TECHSPEC® Nd:YAG Harmonic Separators have a beamsplitter coating on the first surface, which reflects at least one wavelength and transmits another. The beamsplitter coating features greater than 95% transmission. The second surface has an anti-reflective coating to minimize losses from reflection. Designed for integration at 45° angle of incidence, the harmonic separators are manufactured using a precision λ/10 fused silica substrate that offers excellent optical and thermal performance and stability, along with a surface quality of 10-5. The RoHS compliant mirrors have a thickness of 6.35 ±0.20mm, plate construction, and a clear aperture of greater than 85%.
TECHSPEC® Nd:YAG Harmonic Separators are available in multiple wavelength configurations for maximum system design flexibility. Fourteen models offer diameters of 12.70mm and 25.40mm at common Nd:YAG wavelengths of 1064nm, 532nm, 355nm and 266nm. TECHSPEC® Nd:YAG Harmonic Separators are in-stock and available for immediate delivery.
About Edmund Optics:
Edmund Optics® is a leading supplier of optics, imaging, and photonics technology for the Life Sciences, Biomedical, Semiconductor, R&D, and Defense markets around the globe. Edmund Optics designs and manufactures a wide array of multi-element lenses, lens coatings, imaging systems, and optomechanical equipment, while supporting OEM applications with volume production of both stock and custom products. Edmund Optics’ state-of-the-art manufacturing capabilities, combined with its global distribution network, has earned it the position of the world’s largest supplier of off-the-shelf optical components. Customers can purchase items by calling 1-800-363-1992, via the catalog or the website at www.edmundoptics.com.